Technical FAQs

Ask a Question

What is the degree of protection for the keyed selector switch in the 16MM line.

This unit is rated
NEMA type 1, 4, 4X
Conforming to IEC60529 & NF C 20-010
Conforming to UL 50 & CSA C22.2 No. 94
IP65


CTA-ID : 2025372
Was this helpful?
What can we do to improve the information ?