Technical FAQs

Ask a Question

What are the pin outs for the cable that comes with ATV58 Type N remote mount keypad display kit VW3A58837?

There are straight through connections from pins 3,4, 6 and 7 of the female DB9 end connector to pins 3, 4, 6 and 7 of the male DB9 end connector.
See attached drawing 52017-820 for more details.

CTA-ID : 2025698
Was this helpful?
What can we do to improve the information ?