Technical FAQs

Ask a Question

Reference 16205 multi 9 breaker. If it is designed for use in the European market, does it have VDE/TUV/etc ratings?

This product does not have the VDE/TUV marking. Then, we have no certification VDE for it. The ID which has the VDE marking are the 10, 30 and 300mA (German references, for 40A 2P the reference is 12231 for 30mA and 12234 for 300mA).
In 100mA (ref 16205), we will have only reference without VDE/TUV label. Please note: none of these references are supported in the USA.

CTA-ID : 2025471
Was this helpful?
What can we do to improve the information ?