Technical FAQs

Ask a Question

What is the temperature rating for the lugs a PA, PF, PH, PE and PX Breaker?

All circuit breakers are rated for termination at 75 degrees C.


CTA-ID : 2025669
Was this helpful?
What can we do to improve the information ?