Technical FAQs

Ask a Question

Can a straight piece of I Line AP30610 Busway connect to I Line AP306G10 Busway ?

Issue:
Can a  straight piece of I Line AP30610  Busway  connect to I Line  AP306G10 Busway ? 

Product Line:
I Line Busway

Environment:
Application

Cause:
Installation

Resolution:
No, the AP306G10 Busway has a special connector at the joint for the integral ground feature. The AP30610 Busway does not have the Integral ground feature, so the two pieces are not compatible .


CTA-ID : 2025666
Was this helpful?
What can we do to improve the information ?