Technical FAQs

Ask a Question

Who provides support for lifting magnet product lines (e.g., Class 6809, 6810, etc)?

Square D / Schneider sold this product line in 1984 to O.S. Walker Company, Worchester , MA.   Contact 1-800-9624638 .   Only the lifting magnet line was sold to Walker,  not the magnet controllers.  

The magnet controller portion of this business was divested in 2003 to E. C. & M , St. Matthews , SC .  Call 1-800-240-1230 for technical support.

CTA-ID : 2025668
Was this helpful?
What can we do to improve the information ?