Technical FAQs

Ask a Question

Can the Type H circuit breaker be used in the HCN I-Line panel?

Issue:
Can the Type H circuit breaker be used in the HCN I-Line panel?

Product Line:
Panelboards

Environment:
I-Line HCN

Cause:
Fit

Resolution:
Yes the type H breaker can be used in the HCN I-Line panel


CTA-ID : 2025468

Was this helpful?
What can we do to improve the information ?