Technical FAQs

Ask a Question

Is there a 10-12inch long lever arm for a 9007 limit switch?<br />

9007FA7 is spring steel, 12 inches long, similar to those shown on page 19-10 of the 172 Digest. 9007FA10 uses a Delrin rod, 17 1/2`` long that could be cut. Alternately, the 9007R16 or R17 may be fitted with customer supplied rod or keyway, also and fitted with optional rollers 9007R18, 19, or 20..



CTA-ID : 12023
Was this helpful?
What can we do to improve the information ?