Technical FAQs

Ask a Question

What is the part number for an arm for the ZCKD16?<br /><br />

The ZCKD16uses the ZCKY16 lever arm, which currently is available. The head without the lever attached, however, is not available as a separate part.

CTA-ID : 2018480
Was this helpful?
What can we do to improve the information ?