Technical FAQs

Ask a Question

What is the mounting screw part number for the stationary contacts on the Class 8536 Type SE__ NEMA size 3 starter?

Screw assembly part number 21916-20140, includes split washer.


CTA-ID : 2025329
Was this helpful?
What can we do to improve the information ?