Technical FAQs

Ask a Question

What is the temperature rating of the ZCKJ1 and the ZCKJ15

The ZCKJ1 is -25 Deg C to 70 deg C. The ZCKJ15 is -40 deg C to 120 deg C


CTA-ID : 2025682
Was this helpful?
What can we do to improve the information ?