Technical FAQs

Ask a Question

What type of door latching is provided on the very large NEMA 3R/12 NQOD panelboard enclosures and does Square D offer 3 point latching on doors that are 89`` inches high?

A large NEMA 12/3R door offers a handle in the middle and 1/4 turn fasteners on top and bottom, but no true 3 point latching is available.

CTA-ID : 2025651
Was this helpful?
What can we do to improve the information ?