Technical FAQs

Ask a Question

What is the torque requirement for the control wiring terminal block on GFM100FA, GFM100FI, and GFM250?

The recommended torque is 3 - 4 lb-in. The terminal screws on the add on ground fault modules are 2-56 threads.

CTA-ID : 2025455
Was this helpful?
What can we do to improve the information ?