Technical FAQs

Ask a Question

What is the consumption of the control coil for the Class 8903 Type L lighting contactor?

Based on quantity of poles provided as listed below:

2 - 6 pole devices at 60 hertz = Inrush 150 vA, Sealed 30 vA.
2 - 6 pole devices at 50 hertz = Inrush 140 vA, Sealed 30 vA.

8 - 12 pole devices at 60 hertz = Inrush 180 vA, Sealed 35 vA.
8 - 12 pole devices at 50 hertz = Inrush 170 vA, Sealed 35 vA.


CTA-ID : 4857
Was this helpful?
What can we do to improve the information ?