Technical FAQs

Ask a Question

What type of fuse does a QMB361T require?

Issue:
Product Design Features 

Product Line:
Heavy Duty Safety Switches

Environment:
Class R fuse kits 

Cause:
Application

Resolution:
This switch can be used with Class H, K, J or R Depending on the Short Circuit Current Rating(SCCR), SEE the Wiring diagram on the switch for correct fuses associated with SCCR level. Class R fuse should be used with a rejection kit QMB36R.


 
Was this helpful?
What can we do to improve the information ?