Technical FAQs

Ask a Question

Are the EZM 125amp Meter Socket branch devices available in a 2 position device?

Issue:
Current Design features

Product Line:
EZM Metering

Environment:
Number of meter sockets

Cause:
Additional meter sockets in one device

Resolution:

No, the 125amp EZM branch devices are available with a minimum of 3 meter sockets only.


CTA-ID : 2025639
Was this helpful?
What can we do to improve the information ?