Technical FAQs

Ask a Question

What is the cover only for the 9037EG8 float switch

The catalog number is 65079-701-50. To get the correct lable on the cover it is necessary to identify class and type


CTA-ID : 14085
Was this helpful?
What can we do to improve the information ?