Technical FAQs

Ask a Question

How many and what configuration are the contacts on the LUFN20?

This auxiliary contact module is supplied with two normally open contacts with terminal identifications of 33 & 34 and 43 & 44.


CTA-ID : 2025630
Was this helpful?
What can we do to improve the information ?