Technical FAQs

Ask a Question

What is the replacement 240 volt coil for a Type SE NEMA Size 3 contactor or starter?

For 2 & 3 pole devices 31074-400-47 for 60 hertz or 31074-400-48 for 50 hertz. For 4 & 5 pole devices 31091-400-47 for 60 hertz or 31091-400-48 for 50 hertz.


CTA-ID : 4782
Was this helpful?
What can we do to improve the information ?