Technical FAQs

Ask a Question

What is the part# for the filler plate included in N600SFBJ subfeed circuit breaker kit?

Issue:
What is the part number for the filler plate included in the N600SFBJ subfeed circuit breaker kit?

Product Line:
NF Panelboards and Accessories

Environment:
Installation/maintenance

Cause:
Part number

Resolution:
80113-228-03 plate
(4) 80025-067-01 screws

(NOTE:  Although the filler plate is still available, the N600SFBJ subfeed kit which was for the older, Series 0 NF panelboards is now obsolete and no longer available, no replacement.  


CTA-ID : 2025767
Was this helpful?
What can we do to improve the information ?