Technical FAQs

Ask a Question

What type fuses can be installed into a QMB362TW?

Product design feature

Product Line:

Selection of fuse type

Class H or K  fuses can be installed as standard.
Class J fuses can be installed by relocating the Load Base Assembly to the alternate Class J location marked in the switch.
Class R fuses can be installed with field installation of the QMB60R Class R Fuse Kit.
Was this helpful?
What can we do to improve the information ?