Technical FAQs

Ask a Question

My contractor is wanting to put 3/0 conductor on a unit mounted Powerpact R frame circuit breaker. What would the lug be for this?

The lug to use is an AL2500RK. It will accommodate (1) #1/0 AWG - 750 kcmil.

CTA-ID : 2025614
Was this helpful?
What can we do to improve the information ?