Technical FAQs

Ask a Question

What is the maximum output frequency for the Altivar 58 drive?

The maximum setting for output frequency is 500 Hz.

Some motors and/or loads may not be suited for operation above
the nameplate motor speed and frequency. Consult the motor
manufacturer before operating the motor above the rated speed.
Failure to follow this instruction can result in injury or
equipment damage.

CTA-ID : 2025754
Was this helpful?
What can we do to improve the information ?