Technical FAQs

Ask a Question

Can an HVL/cc switch have 6 cables per phase?

Yes, but this is very uncommon. The enclosure must be selected to be 29.50`` wide and 2 additional field shapers must be tagged into the pricing. Each field shaper will accommodate 2 lugs. The 3 shapers will accept the total of 6 cables.

CTA-ID : 2025608
Was this helpful?
What can we do to improve the information ?