Technical FAQs

Ask a Question

What are the dimensions of an MHC50VS and MHC50S?

They are both 50.12 H X 20.12 W. The difference is the door opening. VENTED TRIMS SUCH AS THE MHC50VS ARE ONLY USED ON PANELS RATED HIGHER THAN 225A.


CTA-ID : 2025605
Was this helpful?
What can we do to improve the information ?