Technical FAQs

Ask a Question

Is the Class 8536 Type SF_ starter with melting alloy overload relay available with slow trip class 30 thermal units?

No, the NEMA size 4 starter is configured as standard for trip class 20 or factory modification form Y81 can be supplied for quick trip class 10.


CTA-ID : 2025144
Was this helpful?
What can we do to improve the information ?