Technical FAQs

Ask a Question

Can 3 normally open auxiliary contacts be mounted on a heavy duty safety switch?

No, the selection is either ``1 normally open 1 normally closed`` or ``2 normally open 2 normally closed.`` Suggest the use of a relay mounted outside the safety switch enclosure for extra contacts..


CTA-ID : 2025753
Was this helpful?
What can we do to improve the information ?