Technical FAQs

Ask a Question

What does the 1214 on a circuit breaker designate?

1214 combines suffixes 1212 and 8002 (auxiliary swtich on right pole 1a1b, copper lugs) It is UL approved.


CTA-ID : 2025751
Was this helpful?
What can we do to improve the information ?