Technical FAQs

Ask a Question

What is the rating of the meter sockets on a UT4R1131B? What does ``mains rating`` refer to, which is listed as 205 amperes in the literature?

The sockets are each rated at 100 amperes. The ``mains rating`` is the result of a diversity factor calculation.


CTA-ID : 2025592
Was this helpful?
What can we do to improve the information ?