Technical FAQs

Ask a Question

What are the restrictions for having the Load Discharge Assembly (LDA) on an HVL/cc switch?

The Load Discharge Assembly (LDA) is only available on 5kV - 17.5kV switches. The SEM mechanism is required and the switch must be upright and have the ground switch option. The LDA cannot be used with load side bus or transformer connections to the right. The LDA is not available with 1200A HVL/cc switches.


CTA-ID : 2026077
Was this helpful?
What can we do to improve the information ?