Technical FAQs

Ask a Question

Can a NEMA device be used in 400 Hz applications even if the control power is 60 Hz separate control ?

No, These devices are rated for 50/60 hertz applications only.


CTA-ID : 2025903
Was this helpful?
What can we do to improve the information ?