Technical FAQs

Ask a Question

Do the 9001 BOC interiors for the 9001 BW** pendant stations include the push buttons?

Yes, push buttons are included as part of the interior; however, the legends are not and must be ordered separately.


CTA-ID : 2025900
Was this helpful?
What can we do to improve the information ?