Technical FAQs

Ask a Question

Does the XACA960 cable sleeve for the XACA pendant station come with the retainer ring that holds it to the top of XACA pendant?

Issue:
Does the XACA960 cable sleeve for the XACA pendant station come with the retainer ring that holds it to the top of XACA pendant?

Product Line:
Pendant Station

Environment:
XAC Standard Duty Pistol Grips

Cause:
Clarify if the retainer ring is included in the part assembly.        
       
Resolution:                                                                 
No, the retainer ring is a separate part: it is part number W40424931.
 
Was this helpful?
What can we do to improve the information ?