Technical FAQs

Ask a Question

Are field installable auxiliary contacts available for an H60XFA?

Issue:
Are field installable auxiliary contacts available for a H60XFA?

Product Line:
Enclosed Molded Case Switch

Environment:
NEMA 7/9 Molded Case Switch

Cause:
Need to add aux contacts to existing H60XFA

Resolution:
No, the switch contains an FA frame molded case switch, which will not accept field installed accessories. Order as H60XFA1212


CTA-ID : 2025748
Was this helpful?
What can we do to improve the information ?