Technical FAQs

Ask a Question

What is the maximum number of auxiliary contacts that can be assembled on the Class 8536 Type SC_ NEMA Size 1 starter?

Issue:     
Adding multiple auxiliary contacts to a NEMA class 8536 starter

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Adding auxiliary contacts to a NEMA starter

Resolution:
Up to five auxiliary contacts can be added; one internal and four external. This is in addition to the normally open holding circuit contact which is provided as standard.


CTA-ID : 2025720
Was this helpful?
What can we do to improve the information ?