Technical FAQs

Ask a Question

What is the lug size on a PBQ3640GR plug-in unit?

There are two (2) lugs per phase and neutral that will each accommodate wires from 3/0 up to 600kcmil.


CTA-ID : 2025577
Was this helpful?
What can we do to improve the information ?