Technical FAQs

Ask a Question

Does the DB Chopper for the Altivar 58 turn on when the drive is idle or only when it is running?

The ATV58 does not gate the DB transistor unles it is also gating the IGBT`s.


CTA-ID : 2025431
Was this helpful?
What can we do to improve the information ?