Technical FAQs

Ask a Question

Does the Altivar 31 DB Chopper turn on when the drive is idle or only when it is running?

The ATV31 starts the DB transistor when the bus voltage is about 383 volts on 208-230 VAC drives and about 766 VDC for 460-480 VAC drives, even if the drive is not running the motor.

CTA-ID : 2025320
Was this helpful?
What can we do to improve the information ?