Technical FAQs

Ask a Question

Customer has underfloor duct. Can he get the DM1, DM2, DSC112, DBDP, G149923 & G1480 units?

Issue:
Selection


Product Line:
Wire Management

Environment:
NFPA 70 Art.354, Art. 356; UL884; UL209

Cause:
Changes to usage of a space can drive the need to modify existing underfloor duct installations.

Resolution:
The underfloor duct and its associated service fitting are now obsolete and no longer available.


CTA-ID : 2025428
Was this helpful?
What can we do to improve the information ?