Technical FAQs

Ask a Question

When adding an EZML332400 branch unit to an existing EZM3800CB circuit breaker main, is additional hardware needed, such as tie bars, bolts, etc?

The hardware needed to connect EZM components together comes included with the units.

CTA-ID : 2025110
Was this helpful?
What can we do to improve the information ?