Technical FAQs

Ask a Question

What is the part number for the ATV58HC10N4XZU, ATV58HC13N4XZU, ATV58HC59N4XZU and ATV58HC19N4XZU fan kit?

There are two general types of fan kits.
There are heatsink fan kits that include fans mounted on the back of the drive to direct air across the heatsink.
There are internal fan kits that include fans mounted inside the drive that direct air across capacitors and circuit boards in the drive.
The ATV58HC10N4ZXU drive uses heatsink fan kit VZ3V3808.
The ATV58HC13N4XZU, ATV58HC59N4XZU and ATV58HC19N4XZU use heatsink fan kit VZ3V3809.
The ATV58HC19N4XZU drive has 2 internal fan kits. They are VZ3V3818 and VZ3V3819.
The ATV58HC10N4XZU, ATV58HC13N4XZU and ATV58HC59N4XZU drives only use the internal kit VZ3V3818.

CTA-ID : 2025042
Was this helpful?
What can we do to improve the information ?