Technical FAQs

Ask a Question

Can a QO or HOM 2-pole GFI work on a 2-wire system with a ground but without a load neutral?

Yes, it will work just fine. Note the white curly wire should still be terminated on the panel neutral, and the load ground wire should be terminated on the panel ground bar.

CTA-ID : 2024716
Was this helpful?
What can we do to improve the information ?