Technical FAQs

Ask a Question

What is the replacement vault handle for a NA1200AWK Series E2 Circuit Breaker Enclosure?

The replacement vault handle is 80121-063-50 NOTE: The NA1200AWK is shipped without the vault handle installed. The vault handle assembly and installation instructions are shipped inside of the enclosure, taped to the bottom of the enclosure, for field installation.


CTA-ID : 2025318
Was this helpful?
What can we do to improve the information ?