Technical FAQs

Ask a Question

What is the difference between a ZB2BE101and ZB2BE1016?

Issue:
What is the difference between a ZB2BE101and ZB2BE1016?

Product Line:
Push Buttons

Environment:
All Products

Cause:
Product Features

Resolution:
ZB2BE101 is 1 normally open standard contact block.
ZB2BE1016 is 1 normally open contact and ZB2BE1026 is 1 normally closed contact with gold flashed contacts for use with low current / low voltage. 5-24 volt 0.1-100mA


CTA-ID : 2025316
Was this helpful?
What can we do to improve the information ?