Technical FAQs

Ask a Question

Is the H60XFA a CSA certified device?

Issue:
Is the H60XFA a CSA certified device?

Product Line:
Hazardous location enclosed molded case switch

Environment:
UL, CSA and cULus standards

Cause:
Understanding what standards are met.

Resolution:
This device has been labeled as CSA certified and UL listed. It is currently labeled cULus.


CTA-ID : 2024691
Was this helpful?
What can we do to improve the information ?