Technical FAQs

Ask a Question

Can the Class 8736 Type SE__ vertically arranged reversing starter be field converted to a horizontal arrangement?

No, the wiring provided with the vertical arrangement will not match for horizontal arrangement. Additionally, it does not use the same mechanical interlock.

CTA-ID : 2024925
Was this helpful?
What can we do to improve the information ?