Technical FAQs

Ask a Question

For the XY2CH cable pull switches, is a connector required to connect the cable to the switch?

No, the head of the switch hole in the shaft. Extend the cable through the shaft and rotate the shaft several turns to put tension on the cable. The latching mechanism will prevent the shaft from unwinding. While no additional hardware is required, the cable can also be connected with a cable clamp.


CTA-ID : 2024676
Was this helpful?
What can we do to improve the information ?