Technical FAQs

Ask a Question

Can the QMB3400LA, 400amp Series D2 circuit breaker unit be obtained with a 225A factory installed breaker?

Issue:
Product Availability

Product Line:
QMB Circuit Breaker Devices

Environment:
Breaker Ampere rating

Cause:
Application

Resolution:
Yes, use the catalog number QMB3225LA for a factory installed 225A circuit breaker. Also, the plug-on extension assembly, part number QMB310EX, will be required for the older Panelboard Type QW(38-inch Wide) with flat bus.



CTA-ID : 2025298
Was this helpful?
What can we do to improve the information ?