Technical FAQs

Ask a Question

Can 1 and 2 pole, 15 to 60 amp QO-GFI and QOB-GFI breakers be used in the Powerbus 225 - ``Ready-To-Assemble`` Plug In Unit Enclosures?<br />

Yes, 1 and 2 pole, 15 to 60 amp QO-GFI and QOB-GFI breakers be used in the Powerbus 225 - ``Ready-To-Assemble`` Plug In Unit Enclosures


CTA-ID : 2024655
Was this helpful?
What can we do to improve the information ?