Technical FAQs

Ask a Question

Can 1, 2 and 3 pole QO and QOB breakers be used in the Powerbus 225 - ``Ready-To-Assemble`` Plug in Unit Enclosures?<br />

Yes, you can install QO or QOB breakers that are 1, 2 or 3 poles into the ``Ready-To-Assemble`` Plug in Unit Enclosures


CTA-ID : 2024654
Was this helpful?
What can we do to improve the information ?